示例:ChartRadix 属性

Private Sub RandomRadix() Dim r As RSTradixOptions Select Case Int(Rnd * 3) Case 0 Trend1.Radix = rstRadixDecimal Case 1 Trend1.Radix = rstRadixHex Case 2 Trend1.Radix = rstRadixOctal End Select r = Trend1.Radix Select Case r Case rstRadixDecimal MsgBox "Decimal" Case rstRadixHex MsgBox "Hex" Case rstRadixOctal MsgBox "Octal" End Select ' Show some of the affected numbers Trend1.DisplayLineLegend = True Trend1.DisplayMinMax = True Trend1.DisplayPenValues = True End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal