示例:添加笔

Dim pen1, pen2, pen3 As pen Private Sub AddPens() Dim Ps as Pens Set Ps = Trendx1.Pens ' The tag value identifies the pen ' it must be unique within the control. Set pen1 = Ps.Add("Tag0", "Temp 1", "Deg F", 0, 100) Set pen2 = Ps.Add("Tag1", "Pump 1", "Volts", 0, 100) Set pen3 = Ps.Add("Tag2", "Current", "Amps", 0, 100) End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal