订阅主题

Private Sub Subscribe() On Error GoTo errExit Dim retCode As MqttSubscriptionCode Dim subOption As MQTTSubscribeOption Set subOption = mFactory.CreateSubscribeOption subOption.QoS = MqttQoS2 subOption.Identifier = 10 subOption.Topic = "SE" retCode = mClient.Subscribe(subOption) Exit Sub errExit: MsgBox err.Description End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal