示例:移除文件夹

本示例用于删除指定文件夹中的所有子文件夹。这也会删除其全部子文件夹和标签。
Sub RemoveFolders(sFolderName As String) On Error GoTo Err_Handler Dim oFolder As Folder Dim oFolders As Folders Set oFolder = TagDB.GetFolder(sFolderName) Set oFolders = oFolder.Folders 'Delete the subfolders in specified folder. Do While oFolders.Count > 0 oFolders.Remove 1 Loop 'Release resources associated with the objects. Set oFolder = Nothing Set oFolders = Nothing Exit Sub Err_Handler: 'Release resources associated with the objects. Set oFolder = Nothing Set oFolders = Nothing MsgBox "Error removing folders." & vbCrLf & vbCrLf & _ Err.Description, vbExclamation, " RemoveFolders" End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal