示例:读取标签值

本示例阐述了读取属于 TagGroup 对象的标签的值。第一个子程序创建了 TagGroup 对象,并对其添加了标签并激活 TagGroup。第二个子程序读取 TagGroup 中标签的值。
Dim WithEvents oGroup As TagGroup Sub SetUpTagGroup() On Error Resume Next Err.Clear If oGroup Is Nothing Then Set oGroup = Application.CreateTagGroup(Me.AreaName, 500) If Err.Number Then LogDiagnosticsMessage "Error creating TagGroup. Error: " _ & Err.Description, ftDiagSeverityError Exit Sub End If oGroup.Add "System\Second" oGroup.Add "System\Minute" oGroup.Active = True End If End Sub Sub GetTagValue() On Error Resume Next Dim oTag As Tag Dim vValue As Variant If Not oGroup Is Nothing Then Set oTag = oGroup.Item("System\Second") Err.Clear vValue = oTag.Value Select Case Err.Number Case 0: MsgBox "System\Second = " & vValue Case tagErrorReadValue: MsgBox "Error to reading tag value. Error: " & _ oTag.LastErrorString Case tagErrorOperationFailed: MsgBox "Failed to read from tag. Error: " & Err.Description End Select End If End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal