示例:列出文件夹名称

本示例用于打印指定文件夹中所有子文件夹的名称。
Sub GetFoldersItem(sFolderName As String) Dim oFolder As Folder Dim oFolders As Folders 'Navigate to the specified folder. Set oFolder = TagDB.RootFolder.Folders.Item(sFolderName) 'Get the folders collection. Set oFolders = oFolder.Folders 'Prints the folder's sibling names. For Each oFolder In oFolders Debug.Print vbTab & oFolder.Name Next oFolder 'Release resources associated with the objects. Set oFolder = Nothing Set oFolders = Nothing End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal