示例:获取同级文件夹

本示例用于获取文件夹的同级文件夹和父级文件夹名称。
Sub GetSiblingsAndParent() Dim oFolder As Folder Dim oFolders As Folders Dim oSibling As Folder Dim sFoldersParentName As String Dim sFolderList As String 'Create folders. TagDB.CreateFolder "Line1\Motor1" TagDB.CreateFolder "Line1\Motor2" TagDB.CreateFolder "Line1\Motor3" 'Set a folder. Set oFolder = TagDB.GetFolder("Line1\Motor1") 'Set the folder parent. Set oFolders = oFolder.Parent 'Set the folders parent name. sFoldersParentName = oFolders.Parent.Name 'Loop through all the folders and build a list. For Each oSibling In oFolders sFolderList = sFolderList & vbTab & oSibling.Name & vbCrLf Next oSibling 'Print the folder siblings. Debug.Print "The folder '" & oFolder.FullName & "' has the following siblings:" _ & vbCrLf & vbCrLf & sFolderList 'Print the folder parent name. Debug.Print "The folder '" & oFolder.FullName & "' has the parent:" _ & vbCrLf & vbCrLf & vbTab & sFoldersParentName 'Release objects. Set oFolder = Nothing Set oFolders = Nothing Set oSibling = Nothing End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal