示例:读取标签的值和数据

本示例阐述如何读取标签的值(包括所有与读取标签的值相关的信息)。第一个子程序创建了 TagGroup 对象,并对其添加了标签并激活 TagGroup。由第二个子程序读取标签的值以及标签的所有数据信息。
Dim WithEvents oGroup As TagGroup Sub SetUpTagGroup() On Error Resume Next Err.Clear If oGroup Is Nothing Then Set oGroup = Application.CreateTagGroup(Me.AreaName, 500) If Err.Number Then LogDiagnosticsMessage "Error creating TagGroup. Error: " _ & Err.Description, ftDiagSeverityError Exit Sub End If oGroup.Add "System\Second" oGroup.Add "System\Minute" oGroup.Active = True End If End Sub Sub ShowTagDataInfo() On Error Resume Next Dim oTag As Tag Dim Value as Variant Dim TimeStamp as Date Dim Quality as tagQualityConstants Dim SubStatus as tagSubStatusConstants Dim Limit as tagLimitConstants If Not oGroup Is Nothing Then Set oTag = oGroup.Item("System\Second") Err.Clear oTag.GetTagData Value, TimeStamp, Quality, SubStatus, Limit, TRUE Select Case Err.Number Case 0: ' Read was successful MsgBox "Tag Name: " & oTag.Name & vbCrLf & _ "Value = " & Value & vbCrLf & _ "Quality = " & Switch(Quality = tagQualityGood, "Good", _ Quality = tagQualityBad, "Bad", _ Quality = tagQualityUncertain, "Uncertain") _ & vbCrLf & _ "Timestamp = " & TimeStamp Case tagErrorReadValue: MsgBox "Error to reading tag value of " & oTag.Name & ". Error: " & _ oTag.LastErrorNumber Case tagErrorOperationFailed: MsgBox "Failed to read from tag " & oTag.Name & ". Error: " & Err.Description End Select End If End Sub
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal