USB tab

If you select a ControlNet, DeviceNet, or EtherNet module, you can view information about the device's USB port by selecting the
USB
tab.
General Information:
Attribute Name
Description
Logical Address
Logical address of the USB interface (slot number in the virtual backplane)
State
State of the USB interface (Initializing, Fault, Initialized, Configured, Ready, and Reserved)
Suspend
The USB interface has been suspended by the host
Disabled
The USB interface has been disabled by the host
Bus Speed
The highest USB bus speed the USB interface supports
OnTheGo Support
USB On The Go (OTG) capability support
Mode
Operating mode (slave/host) of the USB interface, if the interface supports OTG
Interface Counters: Diagnostic information in the USB-CIP layer
Counter Name
Description
Interface Received Good Counter
Number of good USB-CIP transfers received
Interface Received Bad Counter
Number of bad USB-CIP transfers received
Interface Received Dropped Counter
Number of dropped USB-CIP transfers
Interface Transmit Good Counter
Number of USB-CIP transfers sent
Interface Transmit Retry Counter
Number of USB-CIP transfers retried
Interface Transmit Dropped Counter
Number of USB-CIP transfers dropped
Media Counters: Diagnostic information in the USB driver layer
Counter Name
Description
Media Received Byte Counter
Number of bytes received
Media Received Dropped Counter
Number of received bytes dropped
Media Transmit Byte Counter
Number of bytes sent
Media Transmit Dropped Bytes
Number of transmit bytes dropped
Media FIFO Overflow
Number of FIFO (First in First Out) overflows
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal