Connection Manager tab

Select the
Connection Manager
tab to view the connection diagnostic information of this device.
Field
Description
Requests
Number of open/close connection requests this module has received.
Format Rejects
Number of open/close connection requests this module has rejected because the request was not formatted correctly or because some parameter value was not within a supported range of values.
Resource Rejects
Number of open connection requests this module has rejected because the module did not have enough resources (buffers, link bandwidth, or CPU utilization) to honor the request.
Other Rejects
Number of forwarded open/close connection requests a module rejects.
Connection Timeouts
Number of connections not explicitly closed by the connection originator, but closed by this module because they were not being used.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal