Configure a shortcut to connect through a FactoryTalk Linx Gateway remote proxy server

Starting from FactoryTalk Linx version 6.40.00, you can use a shortcut to connect through a FactoryTalk Linx Gateway remote proxy server. This will permit a FactoryTalk software in one system to pass communications to controllers and devices in a different system or network across a computer running FactoryTalk Linx Gateway. The FactoryTalk Linx service can operate in a different FactoryTalk directory than the one used by FactoryTalk Linx Gateway. Data delivery speeds will be from 5% to 50% slower through the proxy server than the system without the proxy server. The tested maximum capacity between a proxy server and a client is as follows:
  • 50 shortcuts
  • 500,000 tags, with a 2 second subscription rate
小贴士:
This data is provided as an example capacity. The test did not verify all value changes that were delivered. Because each system has different operational requirements, testing should be performed to determine how a proposed system will operate.
To configure a shortcut to connect to remote proxy devices
  1. On the proxy server computer, configure:
    1. In the FactoryTalk Linx Network Browser, add a local driver, and then browse devices under the local driver node.
    2. Install FactoryTalk Linx Gateway version 6.31.00 or later, and then enable remote proxy service.
      For more information, refer to Enable remote proxy service in FactoryTalk Linx Gateway Help.
  2. On the proxy client computer, configure:
    1. In the FactoryTalk Linx Network Browser, add one or more remote proxy drivers to connect to the driver you created in the proxy server computer.
      For more information, refer to Remote Devices via Proxy Service in FactoryTalk Linx Help.
    2. In FactoryTalk Administration Console, configure a shortcut to connect to controllers of devices discovered under the remote proxy driver.
      小贴士:
      Unsolicited Message and SLC/PLC connections are not supported.
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal