Configure Remote Proxy Driver dialog

Use the
Configure Remote Proxy Driver
dialog to:
  • Modify the name of the remote proxy driver
  • Modify the IP address or hostname of the remote proxy driver
  • Modify the display name of the remote proxy server
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal