Edit an Ethernet driver

Follow this step to modify an Ethernet driver.
In the
FactoryTalk Linx
Network Browser
, select a driver and then click the
Property
These are the available settings:
  • Discovery method
  • Broadcast method
  • Device List/Range method
  • Name of the driver
  • Edit Tuning settings
  • Edit an item to a list in a driver
  • Copy and paste Device List/Range items
  • Delete a driver
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal