Add Driver dialog

How do I open the Add Driver dialog?
  1. From the
    Network Browser
    , click the
    Add Driver
    icon.
  2. In the
    Available Drivers
    list click the driver you want to add to open the
    General
    tab of the
    Add Driver
    dialog box.
Use the
Add Driver
dialog (General and Advanced tabs) to:
  • Select a Discovery Method for the driver
  • Configure a name for the driver that appears in the root of the
    FactoryTalk Linx
    Network Browser
    topology tree
  • Configure an IP address range for the driver
  • Copy and paste IP address range
  • Delete IP address range
  • Configure the advanced network speed of browsing settings
提供反馈
对本文档有问题或反馈吗? 请在这里提交您的反馈 。
Normal