Add a controller
Add a controller to a project to connect the controller with the project. Add controllers from the
Devices
explorer. - On the explorer bar, select
Devices. - InDevicesexplorer, select
Hamburger Menu, then select
New device. TheAdd device to projectdialog opens. - In theAdd devices to projectdialog, underCategory filter, selectController.
- Select a controller from the list and then selectContinue.
- UnderPending to configure, enter the controller information and then selectFinishto add the controller to the device list.小贴士: Controller names:
- Can contain up to 40 valid characters.
- Can contain only alphanumeric characters and underscores.
- Must begin with a letter or underscore.
- Cannot include consecutive underscores.
- Cannot end with an underscore.
小贴士: Additional options to add a controller from either the:- Device list, at the top of theDevice list, select
Add device. - Executionexplorer
. Select
Hamburger Menu, and then selectAdd controller. In theAdd controllers to projectdialog, select a controller from the catalog list.
提供反馈