- 创建项目
- 对象和变量引用
- 扩展项目
示例:请求/响应模式下的协议配置
这是串行
Port
对象中所包含的 NetLogic 的示例,该对象使用请求/响应模式每 300 毫秒读取一次 Modbus 控制器寄存器值。对于
WriteBytes
方法将通过串行端口发送命令,而对于后续 ReadBytes
方法将等待控制器的响应。如果控制器未在 Timeout
属性指示的时间内做出响应,则会生成异常,且读/写失败。可以从 SerialPortDemoRequestResponseMode.zip 下载示例项目。
public class RuntimeNetlogic1 : BaseNetLogic { private SerialPort serialPort; private PeriodicTask periodicTask; public override void Start() { serialPort = (SerialPort)Owner; periodicTask = new PeriodicTask(Read, 300, Owner); periodicTask.Start(); } private void Read() { try { ReadImpl(); } catch (Exception ex) { Log.Error("Failed to read from Modbus: " + ex); } } private void ReadImpl() { serialPort.WriteBytes(Serialize()); var result = serialPort.ReadBytes(3); if ((result[1] & 0x80) == 0) { result = serialPort.ReadBytes((uint)(result[2] + 2)); Log.Info(Deserialize(result)); } else { Log.Error("Failed to read from Modbus"); } } private byte[] Serialize() { var buffer = new byte[] { 0x01, // UnitId 0x03, // Function code 0x00, // Starting address 0x00, 0x00, // Quantity Of Registers 0x01, 0x84, // CRC 0x0a }; return buffer; } private ushort Deserialize(byte[] buffer) { var first = (ushort)buffer[1]; var second = (ushort)(buffer[0] << 8); return (ushort)(first | second); } }
提供反馈