Upload command

Choose this command to upload from the controller into a project file, using the
The current path is displayed in the Online bar, and you can change it using the Who Active dialog. This is the path that the
Logix Designer
application uses when you choose Go Online, Upload, or Download from the menu, and it appears in the Current Path field when you open the Who Active dialog. The current path is written to any projects you create; use the Who Active dialog to change the path in your project. When you open a project, its communication path becomes the current path.
current communications path.
If there is no project open, the
Logix Designer
application looks for a matching project file in your project directory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal