Lock Controller command
Choose this command to lock the controller. By locking the controller, you prevent other users from being able to perform online editing of routines, and from creating or deleting controller components.
When you have the controller locked, this menu option changes to Unlock Controller. If another user has the controller locked, this menu option is disabled.
Provide Feedback