Import Component > Trend command

Choose this command to open the Import Trend dialog to import the selected trend from the selected .L5K file.
.L5K
A file format used for text files imported and exported by the
Logix Designer
application. An .L5K file contains an ASCII representation of the data for an entire project and, when imported, creates a new project file or overwrites an existing project file. This is in contrast to the .CSV.
The file extension for this format must be .L5K; if you change the extension using a tool like the Windows Explorer, the
Logix Designer
application is not able to import this file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal