Go Online command

Choose this command to go online with the controller, using the current communications path.
The current path is displayed in the Online bar, and you can change it using the Who Active dialog. This is the path that the
Logix Designer
application uses when you choose Go Online, Upload, or Download from the menu, and it appears in the Current Path field when you open the Who Active dialog. The current path is written to any projects you create; use the Who Active dialog to change the path in your project. When you open a project, its communication path becomes the current path.
If no project file is open, the
Logix Designer
application looks for a matching file in your project directory. If the project file cannot be correlated with the controller, the
project file
The file on your hard drive that the
Logix Designer
application uses to store a controller's programming and configuration information. The file extension for this file must be .ACD; if you change the extension using a utility like Windows Explorer, the application is not able to open the file.
Connected to Go Online dialog box appears.
When the application is online, this menu option changes to Go Offline.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal