Close command
Choose this command to close the project file.
project file
The file on your hard drive that the
Logix Designer
application uses to store a controller's programming and configuration information. The file extension for this file must be .ACD; if you change the extension using a utility like Windows Explorer, the application is not able to open the file.If the project has been modified, you are prompted to save the changes.
Provide Feedback