Danger: Unscheduling programs online will affect logic execution

You are attempting to unschedule a program or programs while the system is online by dragging them from the Logical Organizer to the
Unscheduled Programs / Phases
folder in the Controller Organizer. If any of the dragged programs have descendants (child items) in the
Logical Organizer
, the descendants are included with the parent items. Unscheduling programs while online changes the execution of programs and may have unintended consequences.
Select
OK
to unschedule the program(s), or select
Cancel
to leave the program(s) scheduled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal