Importing/Exporting a User-defined Data Type
Use Import/Export from the Data Types folder in the Controller Organizer to import/export a User-defined Data Type.
To import a User-defined Data Type from a previously saved .L5X File:
- Right click on the User-Defined or String folder in the Controller Organizer.
- Choose theImportoption.The Import dialog box appears.
- In the File name field, enter the name (and full path) of the .L5X file that contains the content you want to import.Displays the name of the current tag. If desired, you can rename this tag.You may need to navigate to the appropriate directory to find the file if you do not know its full name and path.
- ClickImportto import the content.The Import Configuration dialog box appears.
- Make the appropriate configuration changes, according to how you would like the content to be imported into your current project.
- ClickOK.
To export a User-defined Data Type in the project to an .L5K or .L5X file:
- From within an open project in the Controller Organizer, select User-defined Data Type or String you wish to export.
- Click the right mouse button and choose theExportoption.The Export dialog box appears.
- In the File name field, enter the name you want to use for the content you are exporting.This is the name of the .L5X file.
- Check or clear the Include all referenced Add-On Instructions and User-Defined Types check box.Note that if this check box is not checked, the export file will not contain referenced Add-On Instructions or User-Defined Data Types that are needed to recreate this instruction. In this case, the project you are importing into must already contain the referenced Add-On Instructions and User-Defined Types or the import will fail.
- ClickExportto export the content.
Provide Feedback