Import/Paste Configuration dialog box - Configure Tag References tab

Use this dialog box to review and configure the tag references for the import.
TIP: To open the Import/Paste Configuration dialog - Tag References tab:
  1. Select
    File > Import Component > <component>
    .
  2. Select a component for import and select
    Open
    .
  3. On the
    Import Content
    pane, select
    Tag References
    .
To view tag references in the Import Content, click
Tags
under the
References
folder. The Details pane displays the tag references in the import content. The list includes any tags directly referenced by any imported logic and tags (through
Alias For
).
If the operation on a tag is set to use the existing tag in the project, then the
Scope
,
Alias For
,
Data Type
, and
Description
boxes show the values from the tag in the project and are unavailable. Otherwise, these fields display the values from the import file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal