Import/Paste Configuration Dialog component messages
The following list describes potential problems that you may encounter while working in the Import/Paste Configuration dialog box. These attention messages are indicated by the red flag icon
in the import content and in the Details pane.
in the import content and in the Details pane.The message indicates the nature of the problem, and, in many cases, suggest a remedy to the issue. You may encounter these issues as soon as the dialog box appears or as a result of changes you make in the dialog box.
References to access limitations include the following:
- Security limitations
- Safety limitations - that is, the project is safety secured
- Ssafety limitation of not being able to modify safety components during import while online in either Run Mode or Program Mode - this includes creating, modifying, or deleting components
- Creation of motion objects online
- Restrictions of routine types in Safety tasks - only Ladder Diagram is allowed in Safety tasks
Click the links below for more information about the following types of messages:
Provide Feedback