Import Configuration Component Properties Dialog - General Tab Overview

Use the Properties dialog box to view more extensive component properties than what is provided on the Details pane. The Properties Dialog box displays properties for the imported component, except in the case of a deleted operation in which case the existing component properties display.
Parameters
Import Value
Displays the import value of the variables listed in the left column or the existing value for deleted items.
Current Operation
Displays the current operation selected for the component, as displayed in the Details pane.
See
Import Configuration Operations
for more details.
Create
Click this button to set the operation for the component to Create.
The Create button appears dimmed when create is not a valid operation (for example, a deleted component). Data can be created if the controller is online.
Discard
Click this button to set the operation for the component to Discard.
The Discard button is unavailable when discard is not a valid operation (for example, for a deleted component).
Close
Click this button to close the dialog without making any change to the currently selected operation.
The Close button is the default button.
Help
Click this button for help on this dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal