Import Configuration Dialog - Component Properties Data Tab Overview

Use the collision dialog box to view data values (data and force data) for non-colliding tags in the import. The Data tab of the properties dialog box displays tag values:
  • If the tag is only defined in the import file and not in the project, the data values from the import file are displayed.
  • If the tag is only defined in the project and not in the import file (such as a deleted tag), then the data values from the project are displayed.
  • If the tag is not defined in the project or the import file (for example, for an Alias tag), then no data values are displayed.
Parameters
Current Operation
Displays the current operation selected for the component, as displayed in the Details pane.
See
Import Configuration Operations
for more details.
Create
Click this button to set the operation for the tag to Create.
Create appears dimmed when create is not a valid operation (for example, a deleted tag). Data can be created if the controller is online.
Discard
Click this button to set the operation for the tag to Discard.
Discard appears dimmed when discard is not a valid operation (for example, for a deleted tag).
Close
Click this button to close the dialog without making any change to the currently selected operation.
The Close button is the default button.
Help
Click this button for help on this dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal