Existing tag or component will be used or rescheduled messages

Existing data type for tag <tag name> will be used and some imported tag data values may be lost.
A tag or referenced tag data type is modified during the import (because an imported User-defined Data Type the tag is based on is not imported) so that the tag data is converted. Any member descriptions are converted as well.
Operation
is set according to
Import configuration operations
rules.
Existing Add-On Instruction for tag <tag name> will be used and some imported tag data values may be lost.
A tag or referenced tag data type is modified during the import (because an imported Add-On Instruction the tag is based on is not imported) so that the tag data is converted. Any member descriptions are converted as well.
Operation
is set according to
Import configuration operations
rules.
Existing <component type> <component name> will be rescheduled on import
The controller is in Program mode,
Operation
is set to
Overwrite
, and the imported program or imported equipment phase collides with a program or phase scheduled in a different task or folder (including the unscheduled, or power-up handler, or fault handler folder).
To create a new <component type>, change the final name.
Operation
is set according to
Import configuration operations
rules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal