Existing or imported logic references new or existing tag or component messages
Existing logic will reference the new tag <tag name> after import
A referenced tag is defined in the import file and the logic in the project has undefined tag references to the same tag name and
Operation
is set to Create
.Project logic references the new tag after import unless the
Final Name
is changed or Operation
is set to Discard
.Operation
is set according to Import configuration operations
rules.Existing logic will reference the new [Add-On Instruction | User-defined Data Type] <component-name> after import.
A referenced Add-On Instruction or User-defined Data Type (which is defined in the import file) has the same name as an undefined Add-On Instruction or User-defined Data Type reference in the project and
Operation
is set to Create
.Project logic references the new Add-On Instruction or new User-defined Data Type after import unless the
Final Name
is changed or Operation
is set to Discard
.Operation
is set according to Import configuration operations
rules.Existing tag <tag name> is referenced by logic in [program | equipment phase]. Existing logic will reference the new [program | equipment phase]-scoped tag after import.
A referenced tag is program-scoped and existing program logic is referring to a controller-scoped tag by the same name and
Operation
is set to Create
.Project logic references the new [program | equipment phase]-scoped tag unless the
Final Name
is changed or Operation
is set to Discard
.Operation
is set according to Import configuration operations
rules..If edits are not finalized, imported logic will reference existing program-scoped tag
For a program import and overwrite of an existing program: a controller-scoped tag is being created (
Operation
is set to Create
) and a program-scoped tag by the same name exists in the project and so Operation
is set to Delete
.If
Finalize Edits
are not selected on the Online Options
dialog box, then the program-scoped tag remains after import and the imported program logic references the existing program-scoped tag.Operation
is set according to Import configuration operations
rules..If edits are not finalized, imported logic will reference existing program-scoped tag
For a program import and overwrite of an existing program: a controller-scoped tag is being created (
Operation
is set to Create
) or a controller-scoped tag by the same name already exists and this program-scoped tag by the same name exists in the project and so Operation
is set to Delete
.If
Finalize Edits
are not selected on the Online Options
dialog box, then the program-scoped tag remains after import and the imported program logic references the existing program-scoped tag.Operation
is set according to Import configuration operations
rules..Provide Feedback