Can't create the specified export file
The specified file could not be created. The error message indicates one of these conditions:
Access denied
If the file already exists, check read/write privileges to it.
In use by another product
The file is being edited by another process. Close the file in the other process to export over it.
Path doesn't exist
Make sure that the path exists. If exporting to a network drive, verify the connection to the network.
Provide Feedback