Function Block Properties dialog box - Parameters tab overview
Use the
Parameters
tab of the Function Block Properties
dialog box to get an overview of all the parameters associated with the selected function block.
TIP:
To open the Function Block Properties dialog - Parameters tab, right-click a function block and select
Properties
.Provide Feedback