Add FBD Element dialog box
Use the
Add FBD Element
dialog box to add input/output references, input/output wire connectors, instructions, and functions to a function block routine. Type the instruction mnemonic to see the closest match. Place the instruction or function in a list or in a group.
NOTE:
To open the FBD Element dialog, select
Add Element
in the Function Block editor.Provide Feedback