Changing FBD or SFC Editor Font and Color Preferences
The
Workstation Options
and Print Options
dialog boxes let you set your font and color preferences for the Logix Designer
application. The Workstation Options
dialog box lets you set your preferences for display on the screen, while the Print Options
dialog box lets you set your preferences for printing. These two can be configured differently, even though the options for the Font/Color categories appear the same on each dialog box.
TIP:
To open the Workstation Options dialog:
- SelectTools > Options.
To open the Print Options dialog:
- SelectFile > Print Options.
The FBD or SFC Editor/Listing Font/Color categories lets you configure font and color for items displayed in the FBD or SFC Editor or on FBD or SFC reports.
Note that the name of the category you see in the options dialog box vary, depending on whether you are setting your workstation display or your print options. For
Workstation Options
, all categories refer to the FBD or SFC Editor
; for Print Options
, they refer to the FBD or SFC Listing
.To change FBD Editor or SFC Editor font and color preferences:
- Open either theWorkstation OptionsorPrint Optionsdialog box.
- Configure the following parameters:
- ItemsTheItemslist includes all of the items you can configure for the specific category; configure each item one at a time
- ColorNote that theSamplearea displays an example of what the selected item looks like with the attributes you have configured.
- ClickOKto accept your changes and close theWorkstation OptionsorPrint Optionsdialog box.
Provide Feedback