Reference Information by Tag
The
By Tag
tab is available when the selected Type is:- Tag
- Data Type
- Module
- Add-On-Instruction
This tab displays the tags that alias the selected tag or data element.The tab also shows tags that alias the aliases, and so on. This view also displays the nesting of User Defined Data Types (UDTs).
Double-click on a row to navigate to the Tag Editor. Right-click to navigate to the
Data Monitor
.Sort each column by clicking on the column header:
Column Header | Description |
|---|---|
Scope | Displays the scope of the tag. |
Tag | Displays the name of the tag having the alias. |
Alias For | Displays the name of the tag having the alias. |
Base Tag | Displays the name of the base tag. |
Provide Feedback