Reference Information by Tag Hierarchy
The
Tag Hierarchy
tab is available only when the selected Type is Tag (without a component specified). This tab shows:
- The tag for which the selected tag is an alias.
- Any tag for which the aliased tag is an alias.
- A tag that is outside of the defined scope in the \<ProgramName>.<TagName> format.
- A tag within the scope as only the tag name.
Provide Feedback