SynchLink Transmit Axis tags deleted

The module configuration cannot be updated while you are online. The module will attempt to consume from the deleted axes until the module configuration is updated offline and downloaded to the controller.This message appears when:
  • you delete an associated axis while the Properties view is open online, or
  • you open the Properties view online after you have deleted an associated axis (in this case, the deleted tag name continues to be displayed in the Properties view)
To resolve this problem, go offline, delete the axis, and download the new configuration to the controller. When you go back online, the configuration will be correct.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal