SynchLink tags deleted
The module configuration has been updated to remove the association with these tags.This message appears when:
- you delete an associated axis while the Properties view is open offline, or
- you open the Properties view offline after you have deleted an associated axis, or
- the Properties view is open and you go from online to offline after you have deleted an associated axis tag
Provide Feedback