Reset the port diagnostic counters
On the
Port Diagnostics
dialog box, you can reset the interface and media counters to zero when needed to assist in troubleshooting issues.To reset the port diagnostic counters:
On the
Port Diagnostics
dialog box, click Reset Counters
. The interface and media counter values on the module reset to zero and the values displayed in the dialog box update with the current counter values.Provide Feedback