Ratio between Continuous Task and Service Communication

The table shows the ratio between the continuous task and service communication at various system overhead time slices for
Logix Designer
version 21 or later.
Time slice
Continuous task duration
Service communication duration
10%
9 ms
1 ms
20%
4 ms
1 ms
25%
3 ms
1 ms
33%
2 ms
1 ms
50%
1 ms
1 ms
66%
1 ms
2 ms
75%
1 ms
3 ms
80%
1 ms
4 ms
90%
1 ms
9 ms
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal