Port Diagnostics dialog box parameters
The
Port Diagnostics
dialog box includes the following parameters.Parameter | Description |
Interface Counters | Values only appear when the controller is online.
|
Media Counters | Values only appear when the controller is online.
|
Reset Counters | Sets the interface and media counter values on the controller to zero and updates the values displayed in the dialog box with the current counter values. Reset Counters is only enabled when the controller is online. |
Provide Feedback