Partner
A module in a chassis that is in the same slot position as a module in the corresponding chassis. A module in the primary chassis can have a partner in the secondary chassis, and likewise a module in the secondary chassis can have a partner in the primary chassis.
Provide Feedback