No support of Ethernet port configured modules with redundancy
For the ControlLogix 5580 and GuardLogix 5580 controllers, redundancy does not support modules under the controller's Ethernet front port. Select
OK
and remove all modules under the controller's Ethernet front port in the I/O configuration. Provide Feedback