Motor catalog number error

No motor is available for the associated IDM or more than one motor is available for the associated IDM.
Check your configuration to make sure that at least one motor but not more than one motor is associated to the IDM and apply your changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal