Low Application Memory

The Logix Designer application is low on application memory for one of these reasons:
  • Total Free - the amount of free virtual memory is above the application limit.
  • Largest Free Block - the largest free block of available virtual memory is above the application limit.
  • Number of Free Blocks - the number of free blocks of virtual memory that are over a size limit is above the application limit.
  • Total Allocated Memory - the combined amount of committed and reserved virtual memory is above the application limit.
Save your work and close windows to free application memory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal