Failed to modify priority level. Index out of range.

The Priority 1 or Priority 2 setting in the Controller Properties - Advanced Time Sync dialog box is out of range. The priority values range from 0...255. The highest priority is 0. Select a value within the specified range and click Apply.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal