Failed to load the Configuration pages
There was a problem loading the tabbed dialog box pages for the configuration of the module. This class is not registered.
The tab could not be created. Check the length of the path in which you installed the Logix Designer application. It should not be greater than 100 characters in length.
Provide Feedback