Failed to launch RSNetWorx for EtherNet/IP program file

RSNetWorx for EtherNet/IP could not be launched.
An error occurred when either locating the RSNetWorx for EtherNet/IP program file or executing it. Refer to the message box for the exact cause of the error.
If this problem continues, launch RSNetWorx for EtherNet/IP manually using the Start > Programs option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal