Failed to create ControlNet file

The ControlNet file could not be created.
An error occurred while creating either the folder or file. Refer to the message box for the exact cause of the error.
If this problem continues, create the file manually using RSNetWorx for ControlNet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal