Error could not load from nonvolatile memory
Nonvolatile memory is not present or you do not have sufficient privileges to load the controller image from nonvolatile memory. This error appears when you are attempting to load a project to a controller from a memory card under one of the following circumstances:
- The memory card is not present or is improperly inserted.
- You do not have the privileges to load the controller image from nonvolatile memory.
To complete the load operation, ensure that the memory card is present and is properly inserted into the controller. Also verify with your security administrator that you have sufficient privileges to load the controller image from nonvolatile memory.
Provide Feedback