Electronic Key Passed Fault

Despite passing the electronic keying test, the module being connected to does not have the same features or settings as the module specified in the I/O configuration tree and does not support the connection or service being attempted.
Check the module in use and verify that it exactly matches the module specified in the I/O configuration tree of the
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal